does T4240 can use two srio port as the same time?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

does T4240 can use two srio port as the same time?

466 Views
xinjiezhang
Contributor I

if the 2 srio port can use same times,the ID is same?@

0 Kudos
1 Reply

386 Views
ufedor
NXP Employee
NXP Employee

Yes, the T4240 supports SerDes configuration when two SRIO controllers are used simultaneously.

0 Kudos