AnsweredAssumed Answered

P2020 - Power Consumption

Question asked by Michael Kachalov on Jan 21, 2016
Latest reply on Jan 22, 2016 by alexander.yakovlev

Hello,

 

I am looking at the P2020EC datasheet rev 2 08/2013, dual e500 core device. The data listed in Table 5 (under section 2.3) 'P2020 Core Power Consumption,' is that for a single core or for both cores? That is, a maximum power dissipation of 6.1W at core frequency 800MHz is listed. Would the total consumption of both cores be 6.1W or 12.2W?

 

Thanks

Outcomes