i.MX6Q controller that is placed in CPU2 is Rev1 (or Rev1.3)…?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q controller that is placed in CPU2 is Rev1 (or Rev1.3)…?

469 Views
mithunpsappanna
Contributor I

Hi,

Please help to know MCIMX6QAICPU2 daughter card has i.MX6Q controller that is placed in CPU2 is Rev1 (or Rev1.3)…?

Thanks & Regards

mithun@

0 Kudos
2 Replies

378 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Mithun,

We are using the MCIMX6Q6AVT10AC  the letter C it is the value for the version so it is REV 1.2


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

378 Views
mithunpsappanna
Contributor I

Dear Jaime.

Thanks & Regards

Mitun P S

Mob: +91 7899111606

Dir: +91 080- 40604201

www.em.avnetasia.com<http://www.em.avnetasia.com/>;

0 Kudos