AnsweredAssumed Answered

Unable to boot from the QuadSPI memory on the i.MX 6 Solo X Sabre-sd eval board.

Question asked by ken donna on Jan 20, 2016
Latest reply on Jan 22, 2016 by ken donna

I do have a working SD card that has a newly built U-boot, .dtb files and zImage file running 3.14.52-1.1.0_ga release of the kernel  and u-boot 2015.04.

 

I am trying to load a u-boot image on to the QSPI memory that is on the eval board.

 

Here is what I have done:

- Added the following line to the end of conf/local.conf file : "UBOOT_CONFIG = "qspi2" "

- Built a new u-boot.imx file by running the following command:

  MACHINE=imx6sxsabresd bitbake -c deploy u-boot-imx

this is being done in the same build tree as the one used previously to build linux and the original uboot for the SD card.

 

- This created a new u-boot.imx file which was copied to the VFAT partition of the SD card and renamed as "m4_qspi.bin"

 

- booted the Eval board to the SD card and copied the m4_qspi.bin file to the QuadSPI memory as follow:

  run update_m4_from_sd

 

which produced the following results showing that it was successfully copied:

=> run update_m4_from_sd

SF: Detected N25Q256 with page size 256 Bytes, erase size 4 KiB, total 32 MiB

reading m4_qspi.bin

383024 bytes read in 74 ms (4.9 MiB/s)

SF: 393216 bytes @ 0x0 Erased: OK

SF: 383024 bytes @ 0x0 Written: OK

=>

- Turned off the board and change the dip switch settings for SW10,11 and sw12 to the following :

 

SW10: 0 0 0 0 0 0 0 0

SW11: 0 0 0 0 0 0 0 0

SW12: 0 0 0 1 1 0 0 0

 

- Turned the power on and nothing happens on the serial port.

 

Any Suggestions or corrections of this procedure is really appreciated.

 

Kambiz.

Outcomes