MIPI CSI-2 frame dump

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIPI CSI-2 frame dump

Jump to solution
1,448 Views
shajinas
Contributor I

Hello,

I'm exploring MIPI CSI-2 interface in SABRE SD Platform which uses Omnivision ov5640 camera. My understanding on MIPI is very minimum. I wonder, Is there any way in kernel space the captured frame can be dumped/print ?

Thanks for your time..

Regards

Shajin

0 Kudos
1 Solution
976 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shajin

I am not aware of ways of dumping mipi captured frame, probably

one can write own application using sect.20.3.3 Programming Interface

mipi driver attached Linux Manual. Problem is that mipi has not accessible

data frame buffer, as it uses MIPI CSI to IPU Gasket (CSI2IPU), data is passed

directly to IPU. IPU data is processed with DMA (IDMAC). So for dumping

captured frame both MIPI and IPU should be programmed.

Best regards

igor
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
977 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shajin

I am not aware of ways of dumping mipi captured frame, probably

one can write own application using sect.20.3.3 Programming Interface

mipi driver attached Linux Manual. Problem is that mipi has not accessible

data frame buffer, as it uses MIPI CSI to IPU Gasket (CSI2IPU), data is passed

directly to IPU. IPU data is processed with DMA (IDMAC). So for dumping

captured frame both MIPI and IPU should be programmed.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos