IMX6 Quad and Dual Pin Compability

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 Quad and Dual Pin Compability

Jump to solution
1,940 Views
atillametetured
Contributor V

Greetings,

The question is in the title, are IMX6 Quad and Dual pin compatible? Planning to build 2 versions of a product for some cost reductions.

It would be helpful if that is the case.

Best Regards,

Mete

Labels (3)
0 Kudos
1 Solution
1,029 Views
jamesbone
NXP TechSupport
NXP TechSupport

Yes, let me clarify,

IMX6D-Q-S are compatible each other.  

iMX6DL-SL  compatible with each other

View solution in original post

5 Replies
1,029 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Atilla,

Yes,  the i.MX6 Quad/Dual and Solo Lite are Pin  a Pin Compatible and Software Compatible.  This is one of the advantages of the i.MX6 Family.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,029 Views
atillametetured
Contributor V

Hello Jaime,

Just to clarify, IMX6Quad, IMX6Dual, IMX6DualLite, IMX6Solo and IMX6 SoloLite are all pin compatible? Not just

IMX6Q-D-S within each other and IMX6DL-SL witihin each other independently?

Thanks,

Mete

0 Kudos
1,030 Views
jamesbone
NXP TechSupport
NXP TechSupport

Yes, let me clarify,

IMX6D-Q-S are compatible each other.  

iMX6DL-SL  compatible with each other

1,029 Views
atillametetured
Contributor V

Hello Jaime

Ah allright, thanks for the information.

Best Regards,

Mete

0 Kudos
1,029 Views
mrudangshelat
Contributor IV

Hi,

As per datasheet "For Quad core system, connect to VDD_ARM_IN. For Dual core system, may be shorted to GND together with
VDD_ARM23_CAP to reduce leakage.
"
Now I have made a design with Quad core and i would like to replace with Dual core and I have connected VDD_ARM23_IN with VDD_ARM_IN, and I havn't put an option for connecting with GND.

What should i do now?

What are the other changes i need to do while to have compatibility for Dual core and Quad core?

Regards,

Mrudang

0 Kudos