Are there any patches to support BT1120 of CSI for IMX6q ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are there any patches to support BT1120 of CSI for IMX6q ?

Jump to solution
541 Views
adamzhu
Contributor I

It seems  without drivers in original BSP from freescale  to support BT1120 protocal and Just contains BT656 in mxc_v4l2_capture module. Who can tell me how to config the parameters in driver to support BT1120?  Thanks!!

Labels (4)
0 Kudos
1 Solution
403 Views
art
NXP Employee
NXP Employee

Refer to the following thread:

https://community.freescale.com/message/530894#530894

Hope it will be helpful.


Have a great day,
Artur
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
404 Views
art
NXP Employee
NXP Employee

Refer to the following thread:

https://community.freescale.com/message/530894#530894

Hope it will be helpful.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos