HI all:
I connected my bluetooth headset to I.MX6Q_SABRESD, and my BSP is linux-3.0.35, the buletooth headset can listen music ,but when I using the skype to call, the bluetooth headset can not work, I tried to connected the pcm pin of buletooth chip to esai interface on I.MX6Q_SABRESD, but it seems like the codec driver can not support the bluetooth headset communicate with the I.MX6Q_SABRESD,I referenced the i.MX_6_linux_reference_Manual,Unfortunately,I did not find an answer ,what should I do in the driver so that the bluetooth headset can work when I using skype to call another one? thanks a lot,
Hi bo
it may be recommended to try latest 4.x kernels which
may support it better
https://boundarydevices.com/mx6-kernel-4-1-0/
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------