Hi All
Regarding porting prebuilt image into SD card installed in our i.mx6Q platform , I have encountered the following issue.
When Linux prebuilt image is put into SD card , the attached error has come out and then need to stop the operation unsuccessfully.
Target Sabre board P/N : MCIMX6Q-SDP
Host PC OS : Win 7
Linux BSP used(Prebuilt Image) : L3.14.52_1.1.0-ga_images_MX6QDLSOLO.tar
MFG tool used : L3.14.52_1.1.0_ga-mfg-tools.tar
SW6 DIP switch setting : 00001100
Attached are “Error” , HyperTerminal screen shoot and MFG log file.
Appreciated if anyone help to figure out on the issue.
Best Regards
Aye
Original Attachment has been moved to: MfgTool-Log.txt.zip
Hello,
The simplest way to test the system, using demo images is to copy
image to SD card, as described in section 4.3.2 (Copying the full SD
card image) of “i.MX_Linux_User's_Guide.pdf”
http://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOCS
The SD demo images are as following :
fsl-image-gui-x11-imx6qdlsolo.rootfs.sdcard
fsl-image-qt5-x11-imx6qdlsolo.rootfs.sdcard
Please try it first.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------