MPC5674F Differential ADC Test

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5674F Differential ADC Test

Jump to solution
694 Views
u_kayacik
Contributor II

Hi,

 

Currently working on testing MPC5674F's differential adc measuring capabilites. I simply test the DAN0+ and DAN0- with three resistor like below :

128308_128308.pngnbgoI.png

 

 

uint32_t CQueue_0[] =

{

    ( CHANNEL(96)  | B0 | MESSAGE_TAG(RFIFO0)       ),

    ( CHANNEL(10)  | B0 | MESSAGE_TAG(RFIFO0)       ),

    ( CHANNEL(11)  | B0 | MESSAGE_TAG(RFIFO0)       ),

    ( CHANNEL(12)  | B0 | MESSAGE_TAG(RFIFO0)       ),

    ( CHANNEL(13)  | B1 | MESSAGE_TAG(RFIFO0) | EOQ )

};

 

But conversiton results are not much I wait, output on RFIFO0 -> gives in range of 2681 and 4095 (12 bit conversition). I think it can not give 4095 because of voltage difference is at most 3.3 V.

 

Is this test correct to understand the Diff. ADC is just working? If answer is NO, how can I test it easily?

 

 

Not: R2 and R3 is 1K ohm, R1 22K ohm pot.

 

Best regards,

Umit.

Labels (1)
0 Kudos
1 Solution
581 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Both signals must be in range 0 - 5V, its differential voltage then must be from -2.5V to 2.5V (considering PREGAIN 1x).

You have two ADC inputs, for instance DAN0+ and DAN0-.

Both inputs have allowed voltage range from 0V to 5V. Its differential voltage then must be from -2.5V to 2.5V (considering PREGAIN 1x). because (VRH – VRL)/2 is 2.5V.

See datasheet spec:

pastedImage_0.png

Spec 18 means central point. Spec 17 means voltage range.

Thus allowed voltage range for differential input is

<DIFFcmv-DIFFmax/2, DIFFcmv+DIFFmax/2 > for all PREGAINs

Specifically in your case your differential voltage range is around 0 - 3V, thus your measuring saturates at 2.5V and observed codes are right.

View solution in original post

0 Kudos
3 Replies
582 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Both signals must be in range 0 - 5V, its differential voltage then must be from -2.5V to 2.5V (considering PREGAIN 1x).

You have two ADC inputs, for instance DAN0+ and DAN0-.

Both inputs have allowed voltage range from 0V to 5V. Its differential voltage then must be from -2.5V to 2.5V (considering PREGAIN 1x). because (VRH – VRL)/2 is 2.5V.

See datasheet spec:

pastedImage_0.png

Spec 18 means central point. Spec 17 means voltage range.

Thus allowed voltage range for differential input is

<DIFFcmv-DIFFmax/2, DIFFcmv+DIFFmax/2 > for all PREGAINs

Specifically in your case your differential voltage range is around 0 - 3V, thus your measuring saturates at 2.5V and observed codes are right.

0 Kudos
581 Views
u_kayacik
Contributor II

Thank you for your information David,

Could you please show me a simple test to handle differential ADC signals correctly?

Ümit.

0 Kudos
581 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

You may for instance use 2 potentiometers and 2 resistors

One way will be potentiometer and resistor in series creating DAN0+ voltage with range for instance 0.8V-3.3V (according to pot position).

Second way will be the same i.e. potentiometer and resistor in series creating DAN0- voltage with range for instance 0.8V-3.3V

So let’s set up both potentiometers in opposite corners

DAN0+ = 3.3V

DAN0- = 0.8V

DAN0+ - DAN0- = 3.3-0.8 = 2.5V

Second configuration:

DAN0+ = 0.8V

DAN0- = 3.3V

DAN0+ - DAN0- = 0.8-3.3 = -2.5V

This way you will achieve differential voltage range -2.5V - 2.5V.

0 Kudos