iMX6Q+ADV7180: the picture will move up and down when switch TV standard of input between PAL and NTSC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6Q+ADV7180: the picture will move up and down when switch TV standard of input between PAL and NTSC

780 Views
adamzhu
Contributor I

My board is VAB820 (VIA), which based on imx6q , and connect adv7180 to realize parallel capture function. But when I switch the TV mode of input between PAL and NTSC , the picture will move up and down. Is there any solution to fix the problem? Thanks!!

Labels (4)
0 Kudos
3 Replies

515 Views
igorpadykov
NXP Employee
NXP Employee

Hi Adam

seems this is expected behaviour as with switching mode synchronization

will be lost and some time is needed to recover it.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

515 Views
adamzhu
Contributor I

Hi  igorpadykov

      Could you help to explain the phenomenon of move up and down when switch TV mode between PAL and NTSC?

     Thanks!

      Adam

0 Kudos

515 Views
igorpadykov
NXP Employee
NXP Employee

it is moving up and down due to lost synchronization.

~igor

0 Kudos