AnsweredAssumed Answered

?which MCU and driver board to choose

Question asked by Shai Tzr on Jan 14, 2016
Latest reply on Jan 21, 2016 by Jorge_Gonzalez

Hi,

 

I’m looking for some help on which MCU and driver board to choose.

 

Basically I need to control a servo motor and 2 DC motors, as well as “read” a few sensors like Hall Effect sensor (for speed sensing) and a simple CCD/CMOS sensor (for computer vision based navigation).

 

From my research I thought I’d use a TWR-K65F180M + TWR-ELEV + TWR-SMPS-LVFB but it seems that the TWR-SMPS-LVFB won’t be compatible with the K series MCU, is that right? The reason I want the TWR-K65F180M and not the TWR-KV31F120M (or some other TWR based on the V series) is mainly because of the extra SRAM it offers that would be important for the image storing.

 

Any guidance with that?

 

Thanks,

Shai

Outcomes