Hello, I purchased automotive infotainment dualite cpu board last week (MCIMX6DLAICPU2) and built root file system to boot the processor from SD card thru UART debug port, but, i am unable to debug the board. I doubt the switches S1, S2 and S3 that is configured was not correct, can someone please help me to set S1, S2 and S3 correctly??. After puting the SDCARD in the CPU board the cursor moves by one character on Putty.
Thanks,
Guru.
Hi Guudath
for debug steps one can look at
Sharing debug i.mx6 from uboot to kernel to jni with Eclipse
http://cache.nxp.com/files/32bit/doc/app_note/AN4553.pdf
If jtag is used, then switches should be set for Serial Downloader
mode.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------