hello,
I can communicate between the 2 p2041 using the rapidIO.
how can I using the message END API ?
vxworks6.9
Solved! Go to Solution.
Yes, the P2041 can be connected using RapidIO. The P2041 can communicate using this connection. See please the Chapter 4.12 of the RapidIO Interconnect Specification, Revision 2.1 Part 6 (http://www.rapidio.org/specs/current)
There is single limitation for the P2041 and P4080 RapidIO:
The P2041 and P4080 RapidIO endpoint cannot be configured as four 1x ports
See also the following information on NXP Technical Information Centre for RapidIO testing:
See also the following Application Note: AN2923, AN2932 on Application Note.
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Yes, the P2041 can be connected using RapidIO. The P2041 can communicate using this connection. See please the Chapter 4.12 of the RapidIO Interconnect Specification, Revision 2.1 Part 6 (http://www.rapidio.org/specs/current)
There is single limitation for the P2041 and P4080 RapidIO:
The P2041 and P4080 RapidIO endpoint cannot be configured as four 1x ports
See also the following information on NXP Technical Information Centre for RapidIO testing:
See also the following Application Note: AN2923, AN2932 on Application Note.
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
got it ,thanks I will try.