We are using imx6-sabresd board ,and system is android 4.4.2.Using ov5640 camera. |
We want to implement the digital zoom function of camera.
who can tell me how to do?
Hello,
Digital zoom may be performed as image resizing (with interpolation)
via IPU on i.MX6. For more details please refer to IPU driver description in
“i.MX_Linux_Reference_Manual.pdf” and IPU chapter in the i.MX6 Reference
Manual.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I have read this manual, but I still don't know how to achieve digital zoom in the code。
Could you give me an example
Hello
The following may be useful :
rogeriorps/ipu-examples · GitHub
Also You may look at section 6.4.3 (IPU Device Unit test) of
“i.MX_6_Linux_Reference_Manual.pdf”.
http://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOC
Regards,
Yuri.