AnsweredAssumed Answered

Creating s19 file. Target: DSC MC56F8345

Question asked by Davide Arosio on Jan 11, 2016
Latest reply on Feb 26, 2016 by Fiona Kuang

Hi everybody,

Is there a way to create an s19 file from a Codewarrior project? I need this file to program a lot of microcontrollers with the USB Multilink Universal FX programmer. I control this programmer with its command line options. I am using Codewarrior v.8.3 and the target is a DSC microcontroller (MC56F8345). I have also other versions of Codewarrior, so I would be pleased if somebody can suggest me if I am using the correct version of CW. In addition, if it is possible to create the s19 file, would it be possible to read the procedure step by step? Thanks in advance.

Outcomes