AnsweredAssumed Answered

iMX6UL HAB Questions

Question asked by SJA on Jan 8, 2016
Latest reply on Jan 10, 2016 by Yuri Muhin

Can the signed u-boot image be verified on the EVK without CLOSING the SoC

when loading via USB (mfgtools technique)? When attempting this I

consistently see HAB events with INV_ADDRESS CTX_AUTHENTICATION.

 

Does the binary CSF file created using the cst tool have to be padded to the

size specified with CONFIG_CSF_SIZE in the u-boot imximage.cfg file before

being appended to the u-boot image?

 

Does the signed u-boot image need to be padded for 0x1000 alignment?

 

If so, does the size value specified in the CSF script "[Authenticate Data]

Block =" command reflect the u-boot image size before or after padding?

 

Note: We are using the HAB4 CSF Fast Authentication loading the images via

USB

Outcomes