AnsweredAssumed Answered

Freescale meta-java layer support

Question asked by Surendra Dhobale on Jan 8, 2016
Latest reply on Jan 27, 2016 by Surendra Dhobale

Hi,

     I am using QorIQ-SDK-V1.8 for T1040 RDB. I am able to build the test java image on it. It has zero, cacao and jamvm VM. I have java application which is running on the zero vm with this SDK.

But not case with CACAO and JAMVM. In this meta-java, icedtea project has version 2.3.12 and openjdk7_25b30. But currently updated versions available. I am looking to port 2.6.2 icedtea with this meta layer. I have seen the patches are available in the yocto projcet- meta-java layer.

 

but facing issues with compilation of icedtea2.6.2 package.

 

I just want to ask, Is freescale (NXP) maintainaing the repository with this kind of the updated layers.?

 

Or What could be the approch to port the patches in the meta-java or  any openembedded repository to freescale meta-layer patches porting?

 

 

Regards,

Surendra

Outcomes