HI every one
we used yocto setup and linux kernel 3.14.
we compiled individually bitbake gstreamer1.0-plugins-imx/gstreamer1.0-rtsp-server and
we added local.conf file below mentioned lines
IMAGE_INSTALL_append += " gstreamer1.0-plugins-imx"
IMAGE_INSTALL_append += " gstreamer1.0-rtsp-server"
but those are compiled but we want to those lib.so is the part of rootfs image .how we add?
we added fsl-image-machine-test.bb file
gstreamer1.0-plugins-imx \
gstreamer1.0-rtsp-server
bitbake full-image-machine-test
but these libraries are created in below mentioned path
<build_dir>/tmp/sysroots/imx6qsabresd/usr/lib
those libraries are not in the part part of rootfs.sdcard image and rootfs.tar.gz
How its come in the part of rootfs image .
<build_dir>/tmp/deploy/image/imx6a/rootfs--.sdcard
can you explain any body please.we are waiting for your valuable suggestions.
Hello,
You may look at section A.4 (How to select additional packages) of
“Freescale_Yocto_Project_User's_Guide.pdf”; in particular – according to
section A.4.1 (Updating an image) : “Note: You can build packages without
including it in an image, but you must rebuild the image if you want the package
installed automatically on a rootfs.”
http://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOCS
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------