i. MX6 Quad and i. MX6 Dual-Lite/USB eye pattern Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i. MX6 Quad and i. MX6 Dual-Lite/USB eye pattern Configuration

831 Views
soichiyamamoto
Contributor V

Hi,

I develop a trial manufacture board of i. MX6 Quad and i. MX6 Dual-Lite.

I let you output a signal from the following pin and want to observe eye pattern to evaluate the signal quality on the board of USB I/F.

 ・i.MX6 Quad USB_OTG_DN(B6)

 ・i.MX6 Quad USB_OTG_DP(A6)

 ・i.MX6 Dual-Lite USB_OTG_DN(B6)

 ・i.MX6 Dual-Lite USB_OTG_DP(A6)

 ・i.MX6 Dual-Lite USB_H1_DP(E10)

 ・i.MX6 Dual-Lite USB_H1_DN(F10)

Please tell me the register setting to operate the test pattern output by such a use.

Or, please provide it if there is a sample program.

Best Regards,

soichi

Labels (2)
0 Kudos
1 Reply

401 Views
Yuri
NXP Employee
NXP Employee

Hello,

The following from the Community are devoted to USB certification.

I.MX6 series USB Certification Guides

Patch to make i.MX6DQ USB to support test modes for certification test


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos