Update to KDS 3.1.0 a Fail on OS X

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Update to KDS 3.1.0 a Fail on OS X

538 Views
razed11
Contributor V

Any ideas? I followed Erich's directions on the 12-22 post .

123408_123408.pngScreen Shot 2016-01-02 at 4.54.32 PM.png

 

I also reinstalled, fixed the OSX splash screen bug, and tried to update from the archive. Similar errors:

 

123409_123409.pngScreen Shot 2016-01-02 at 5.33.04 PM.png

 

Message was edited by: Kenny Koller  Added more information after upgrade failed from fresh install.

Labels (1)
0 Kudos
2 Replies

359 Views
michalzan
NXP Employee
NXP Employee

Hi Kenny,

why don't you install KDS 3.2?

Kinetis Design Studio Integrated Development Envir|NXP

It is definitely more stable.

Michal

0 Kudos

359 Views
trytohelp
NXP Employee
NXP Employee

Hi Kenny,

I've a Mac and I met some problems to install the V3.1 update.

Running the Install New Software I got some problems (Error message)

At then end I was able to install the update following this process:

    - select Help + Installation Details,

    - select Kinetis Design Studio which displayed 3.0 and click on update,

    - then the V3.1 update was installed and now the system displays V3.1.

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos