Hi,
I am running OBDS on iMX28EVK. NAND Test fails with output given below. Board has one MT29F4G16ABADAWP connected using NAND Flash Socket.
Any help on this?
Regards,
Arun
======================================================
---- Running < NAND > test
Please enter y or Y to confirm
input char is: y
Reset NAND
Read NAND ID for CE0: ID for CE0, is 0x2c, 0xdc, 0x90, 0x95, 0x56
**NAND device unrecognized!
======================================================
Solved! Go to Solution.
Hi Arun
supported parts are provided in file
include/mx28/supported_nand_parts.inl.
So please add necessary record for this NAND
and rebuild OBDS.
Best regards
igor
Hi Arun
supported parts are provided in file
include/mx28/supported_nand_parts.inl
so one can add necessary record.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor,
I am using binary flashed on SD Card.
I have requirement to run OBDS and have the tests pass.
Please let me know steps / procedure to make OBDS NAND test pass on iMX28 EVK.
Regards,
Arun
Hi Arun
supported parts are provided in file
include/mx28/supported_nand_parts.inl.
So please add necessary record for this NAND
and rebuild OBDS.
Best regards
igor
Thanks, igor !
This helps.
Regards,
Arun