Pre and Post build commands only run when Parallel build is disabled, when enabled they do not run.
Is this a bug?
Windows 7 KDS 3
Hi Leif,
pre- and post-build steps work for me with parallel build enabled (using Win7 too). But there is a known issue in case you have custom per-file or per-folder options set, see Traps and Pitfalls: No Hex/Bin/S19 File Created with GNU? | MCU on Eclipse .
This is my setup:
Erich
... At lease it works for some. I guess I will create a test project.
And the link does not apply, i think.
It is very odd, I have two machines same setup same issue. and I am trying to compile the MQX psp and bsp for my board and the pre/post commands only run with parallel buildi off.