How to boot a p1022 proessor from emmc device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to boot a p1022 proessor from emmc device

717 Views
saurabhagarwal
Contributor III

How can I boot a device with p1022 processor from emmc device ? is it possible? 

0 Kudos
2 Replies

598 Views
ufedor
NXP Employee
NXP Employee

Please refer to the application note Booting from On-Chip ROM (eSDHC or eSPI):

http://cache.nxp.com/files/32bit/doc/app_note/AN3659.pdf

0 Kudos

598 Views
saurabhagarwal
Contributor III

While reading the QorIQ SDK 1.8 manual, I understood that we can place the ext2 filesystem and kernel on the SD card, then the kernel can boot up automatically after the board is powered on, given that parameters in u-boot are set.  So. I understood that we can place kernel and file system in sd card.

Where is u-boot stored ?

Can we place u-boot in sd card ?

How to program u-boot. ?

0 Kudos