3.14.28 lvds 显示

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

3.14.28 lvds 显示

611 Views
强王
Contributor IV

环境:

双核,LVDS,分辨率1024*600,内核3.14.28,显示如下,不知道哪里的问题(同样的配置,使用3.10.53显示正常)

屏幕显示如IMG_0827.JPG

Labels (4)
Tags (3)
0 Kudos
1 Reply

397 Views
igorpadykov
NXP Employee
NXP Employee

Hi Qiang

similar 1024x600 lcd is used on boundary devices bsp, so one can look how it is

integrated

linux-imx6/imx6qdl-nitrogen6_max.dtsi at boundary-imx_3.14.28_1.0.0_ga · boundarydevices/linux-imx6 ...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos