understanding iomuxing imx6QD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

understanding iomuxing imx6QD

1,757 Views
srinivasaporam
Contributor II

Hi,

We are working on imx6q processor board and want to understand iopin muxing in detail. for this we have refereed to imx6q-pinfun.h file

for example: it states:

#define MX6QDL_PAD_CSI0_MCLK__IPU1_CSI0_HSYNC   0x25c 0x62c 0x000 0x0 0x0
#define MX6QDL_PAD_CSI0_MCLK__CCM_CLKO1         0x25c 0x62c 0x000 0x3 0x0
#define MX6QDL_PAD_CSI0_MCLK__GPIO5_IO19        0x25c 0x62c 0x000 0x5 0x0
#define MX6QDL_PAD_CSI0_MCLK__ARM_TRACE_CTL     0x25c 0x62c 0x000 0x7 0x0

where it staed that  the pin function ID is a tuple of

<mux_reg      conf_reg      input_reg      mux_mode       input_val>

if i take one example from above let's say :

#define MX6QDL_PAD_CSI0_MCLK__CCM_CLKO1     0x25c 0x62c 0x000 0x3 0x0

if i look the reference manual, then mux-reg for CSI0_MCLK is IOMUXC_SW_MUX_CTL_PAD_CSI0_HSYNC (Address: 20E_0000h base + 25Ch offset = 20E_025Ch) offset is 0x25c

conf_reg for CSI0_MCLK is IOMUXC_SW_PAD_CTL_PAD_CSI0_HSYNC (Address: 20E_0000h base + 62Ch offset = 20E_062Ch), so offset is 0x62c

MUX-Mode i need select from IOMUXC_SW_MUX_CTL_PAD_CSI0_HSYNC whose value 011 (0x3)

So

#define MX6QDL_PAD_CSI0_MCLK__CCM_CLKO1 0x25c 0x62c 0x000 0x3 0x0

in above macro i got 0x25c 0x62c 0x3 but what about values of  input_reg (0x000) and input_val (0x0) ??????? how to get them correctly?????

and also if iam using them in my dts for iomux

for example say :

mipi_csi {

        pinctrl_mipi_csi_1: mipi_csipgrp-1 {

            fsl,pins = <

              

                    MX6QDL_PAD_CSI0_MCLK__CCM_CLKO1    0xb0b1

 

            >;

        };

};

in above 0xb0b1 is the value taken from IOMUXC_SW_PAD_CTL_PAD_CSI0_HSYNC.

which is the value we should take. is taking SW_PAD_CTL_PAD value be sufficient?????

Please reply...

Labels (3)
0 Kudos
Reply
5 Replies

1,126 Views
srinivasaporam
Contributor II

Hi,

I would like understand briefly how to get the values for io pin muxing like

pastedImage_0.png

For ex:

I take taken dts file of some reference design where they are using :

MX6QDL_PAD_GPIO_3__CCM_CLKO2   0x000b0

from the above ,

HYS=0  CMOS input, How we will come to know whether we require CMOS input or schmitt trigger input (or by trial error method)

PUS=00       100K Ohm pull-down  (how to get this value from schematic, whether we require Pull up or pulldown and choose between 100 K PU, 100 K PD, 22K PU, 47K PU ????)

PUE = 0 (how choose between keeper and puller)

PKE= 0  (pull /keeper enable  disable. how choose ????)

Speed =(how to choose the correct speed required?????

DSE (Drive Strength how to choose correct values????)

MX6QDL_PAD_GPIO_3__CCM_CLKO2   0x000b0

whether they have arrived at 0x000b0 by trial and error method or how to derive it exactly ????

0 Kudos
Reply

1,126 Views
srinivasaporam
Contributor II

Hi,

I Checked in Reference Manual, But it is just confusing.

for Some Values like : (as an example)

MX6QDL_PAD_CSI0_DAT12__IPU1_CSI0_DATA120x80000000

Here We need to check SW_PAD_CTL_CSIO_DAT12

Bit 16 -HYS is selectable

Bit 15 14 -PUS

like that. But how they have made bit 31 as 1 (0x80000000)

0 Kudos
Reply

1,126 Views
igorpadykov
NXP Employee
NXP Employee

The 0x80000000 means that the kernel will not touch the PAD settings and

it will use whatever comes from default (or from U-boot in case it was

previously configured in U-boot).

0 Kudos
Reply

1,126 Views
glitch911
Contributor I

Hi,

I know it's been a long time since you replied this question but can you point me to the source of this 0x80000000 value?

More precisely I'd like to know if it's only the PAD_CTL that is unchanged or the MUX_CTL setting as well?

For example MX6QDL_PAD_EIM_D22__GPIO3_IO22 is supposed to set the EIM_D22 PAD as GPIO (ALT5) but after changing u-boot to use USB OTG it seems that PAD_EIM_D22 is now configured as USB_OTG_PWR (ALT4) and MX6QDL_PAD_EIM_D22__GPIO3_IO22 0x80000000 seems to do nothing about that as I still read 4 when typing devregs 0x020e00a8 (MUX_CTL). 

0 Kudos
Reply

1,126 Views
igorpadykov
NXP Employee
NXP Employee

Hi Srinivasa

input_reg and input_val are address offsets for daisy chain register (IOMUXC_xxx_SELECT_INPUT)

and its value (if it presents for that signal). Regarding SW_PAD_CTL_PAD value you should check

description in RM and choose appropriate for your needs value.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply