I can't compile "bsp-nto650-freescale-imx53-qsb-sp1-trunk-201209071552.zip" from the Freescale website in the IDE.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I can't compile "bsp-nto650-freescale-imx53-qsb-sp1-trunk-201209071552.zip" from the Freescale website in the IDE.

426 Views
ballerzhu
Contributor I

Hello,

     I can't compile the BSP of  I.MX53 in the IDE.

It  always presents errors that are "Unable to to find startup: startup-mx53qsb" and

" *** No rule to make target `libinput.a', needed by `D:/QNX-IDE-projectp-freescale-imx53-qsb888-src/src/hardware/devi/mc34708".

I use "bsp-nto650-freescale-imx53-qsb-sp1-trunk-201209071552.zip" from the Freescale website.

Can you help me?

     Thanks very much.

Labels (1)
0 Kudos
1 Reply

284 Views
igorpadykov
NXP Employee
NXP Employee

Hi Baller

this BSP is provided by qnx, suggest to post question on its wiki:

http://community.qnx.com/

I.MX53 QSB Freescale BSPs are based on ltib and located on

Board Support Packages (8)

i.MX53 Quick Start Board|NXP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos