How to enable Broadcom 89810 ETH phy on i.MX6Q-AICPU?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable Broadcom 89810 ETH phy on i.MX6Q-AICPU?

1,127 Views
jiaweiyu
Contributor I

Hello,

I am a new developer on i.MX6Q-AI and now using Freescale YOCTO BSP r14.10.28.

I have three boards on my hand:

  • i.MX6Q-AI CPU board
  • Atheros ETH phy
  • Broadcom ETH phy

The problem is:

I got the Atheros ETH phy running well on CPU board and tested with another set of phy and cpuboard.

But when I connect Broadcom ETH phy to CPU board, it doesnot work properly.

I have tried to include ETH drive in kernel with the cmd "make menuconfig" and find that there is no driver for Broadcom 89810.

What can I do to enable the Broadcom ETH phy?

Thanks and regards

Jerry

Labels (2)
0 Kudos
3 Replies

603 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I hope the following helps.

Broadcom Firmware package


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

603 Views
jiaweiyu
Contributor I

Hi,Y uri

Happy new year!

The firmware seems support only the bcm 4seri es wifi chips and do not include driver for bcm89810.

Any other suggestions for me?

Much thanks

0 Kudos

603 Views
Yuri
NXP Employee
NXP Employee

Hello,

the following may be helpful BroadR-Reach support for i.MX6

Regards,

Yuri.

0 Kudos