Can J-Link Ultra+ be used to flash the firmware- WCT5WTXAUTO.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can J-Link Ultra+ be used to flash the firmware- WCT5WTXAUTO.

Jump to solution
556 Views
sourabhshyampan
Contributor I

I'm working on WCT-5WTXAuto, But I don't have the tool ( multilink) to flash the NFC firmware to the MCU, is it possible to flash the MCU suing J-Link Ultra+ https://www.segger.com/jlink-ultra-plus.html, if yes, what is the procedure to create the image that can be flased using J-link Ultra ?

Labels (1)
0 Kudos
1 Solution
436 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Sourabh

WCT-5WTXAuto is not based on an ARM MCU, J-Link Ultra+ does cannot flash it. You need a USBTAP or Universal Multilink:

http://www.nxp.com/products/software-and-tools/software-development-tools/codewarrior-development-to...

http://www.nxp.com/products/interface-and-connectivity/wireless-connectivity/sub-1-ghz-wireless-solu...

Best Regards

Fiona Kuang

Technical Information & Commercial Support
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
437 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Sourabh

WCT-5WTXAuto is not based on an ARM MCU, J-Link Ultra+ does cannot flash it. You need a USBTAP or Universal Multilink:

http://www.nxp.com/products/software-and-tools/software-development-tools/codewarrior-development-to...

http://www.nxp.com/products/interface-and-connectivity/wireless-connectivity/sub-1-ghz-wireless-solu...

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos