I currently have CodeWarrior for MCU Version: 10.6 Build Id:140329 (Special Edition). I am able to create bareboard projects (with some Processor Expert components).
I do not have the option File -> New -> Processor Expert MQX Lite Project. (as specified in the MQXLite User Guide).
When I try to create a new project, the choices given are: Linux/uCLinux Application Project, Bareboard Project, Embedded Component, Project.., Others..
I also cannot find the MQX Lite Project option under the "Project.." or "Others..." options.
What must I install or change to get the MQX Lite Project option to appear?
Thanks.
Solved! Go to Solution.
Hello wong,
What about your CodeWarrior License ?
Only the Professional CW can use the mqx-lite .
You can check the CW suite reference guide of the attachment .
BR
Alice
Hello HW,
Please check have you install the "MQX-LITE wizard component" here :
Hope it helps
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Have a great day,
Alice Yang
After installing, I do get the MQX-Lite Project when I do a File->New to create new project.
However, if I choose MQX-Lite Project by clicking it, nothing happens. (not even an error message).
(Could be something else which I need to install)
Thanks for the help so far.
Hello
Have you install the MQX4.2 ?
Have a great day,
Alice Yang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Sorry if I sound like I am asking the obvious; what else must I do to be able to add MQX Lite to new or existing projects?
After installing CodeWarrior MQX 4.2 Plug-ins, I still have
a) No respond when I choose to create a new project and then choose MQX Lite.
a) Do not have the category OS when I try to add MQX Lite to an existing project.
(see diagram below)
I already have MQX Plug-ins, MQX 4.0.x Plug-ins, MQX 4.1 Plug-ins, MQX 4.2 Plug-ins and MQX-Lite Project Wizard component all installed when I experience the symptoms described above. See the screen-dump showing the relevant areas of the "Installed Software".
Thanks Alice.
I guess that solves the "mystery".
From your attached "CW reference guide", it seems MQX Lite is only available for Kinetis using Code Warrior Professional license.
I guess I am both on the "wrong" MPU and license since I am using the Code Warrior Eclipse License (Special) for S12Z MPU.
Hi,
You are welcome ! Yes, for the S12Z chips, no matter how , the mqx-lite doesn't support it .
Have a nice day !
Alice