Dear Sirs:
I would like to work with the MC34844A under the following requirements:
Is is possible to reach such voltaje we made several tests but we never reach more than 47V and we are not sure we can fron the datasheet data.
If 60 V( and current mentioned) are reachable please let me know the values of:
L
Cout
Ccomp1
Ccomp2
Rslope
Rpcomp
Rccomp
Thanks in advance
Jorge Domingo
DFAE Freescale
EBV ELEKTRONK
Hi Jorge,
Yes, you can reach up to 60V output with the MC34844A, but not with a VIN of 12V, you would need an input voltage of 28V (with an Iout typ of 0.4A) with the following components values:
L = 120 uH
Cout = 47 uF
Ccomp1 = 8.6 nF
Ccomp2 = 99.5 pF
Rslope = 216 Kohms
Rcomp = 5.6K
Have a great day,
Jose
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------