512 MB DDR3 on Vybrid? Changes to init for DDR controller needed to go from K4B1 to K4B4 Samsung part

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

512 MB DDR3 on Vybrid? Changes to init for DDR controller needed to go from K4B1 to K4B4 Samsung part

831 Views
markwatson
Contributor III

The timing looks the same for the 4 Gb part vs. the 1 Gb  part used on the tower board.  We have successfully made at least three layouts with the K4B1G1646G DDR3 as used on the Tower board.  We added impedance controlled and matched length traces for A13 and A14.  We modified the value in DDR_CR073 to indicate the two additional rows, but Uboot hangs right when it tries to jump to running from RAM.  The new DDR3 part is K4B4G1646B which seems to have the same timing at the old part.  I have reviewed various posts and looked at register contents after a successful boot on the same board with the 128 MB part vs a failed boot with the 512 MB part.  It seems we must be missing something basic.  Any help would be appreciated.

Labels (1)
0 Kudos
2 Replies

499 Views
timesyssupport
Senior Contributor II

Hi Mark,

Unfortunately, we have not yet worked with this DDR part for Vybrid. One thing that comes to mind is that you may need to recalibrate DDR RAM to account for the part change. This thread has more information about a DDR stress test/calibration tool that you can use.

Is there a DDR3 stress test tool for the Vybrid processors?

Thanks,

Timesys Support

499 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can yo help here?

0 Kudos