AnsweredAssumed Answered

Question, NAND chip TC58NVG0S3 use for i.MX25

Question asked by AVNET JAPAN FAE (team share account) on Dec 17, 2015
Latest reply on Jan 7, 2016 by Yuri Muhin

Dear team,

 

A while ago, we received the answer on Toshiba/TC58NVG0S3 NAND chip use for i.MX25 from this community as below.

https://community.freescale.com/thread/379638

 

And it says that Toshiba/TC58NVG0S3 NAND flash chip cannot meet the specification of i.MX25 NFC.

We found the description table entry of “TC58NVG0S3” in your LinuxBSP, L2.6.31_09.12.00, source code.

It is written in nand_device_info_table_type_2[] structure in drivers/mtd/nand/nand_device_info.c file in the LinuxBSP.

If the code has not been tested, I mean whether the table entry of TC58NVG0S3 can really work is not sure,

Then Can I understand the NAND chip might be used as NAND device under the Linux but the NAND chip still cannot be used for Boot device?

 

Thanks,

Miyamoto

Outcomes