About DMA of ECSPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About DMA of ECSPI

Jump to solution
615 Views
takashitakahash
Contributor III

Hi community.

Our customer has below question.

About DMA of ECSPI,
ECSPI by Configu to SPI of the Master, so it is to transmit only.
( Receive is not performed).

TXFIFO side, as to send data using DMA,
RXFIFO side, ignoring overflow, sending doesn't matter?

(For example, Disable to RXFIFO Overflow Interrupt , do not affect the TX processing?)

Labels (1)
0 Kudos
1 Solution
493 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

you are right, RX side can be ignored, possibly disabling

RXFIFO Overflow Interrupt. This should not affect TX processing.

Best regards

igor
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
494 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

you are right, RX side can be ignored, possibly disabling

RXFIFO Overflow Interrupt. This should not affect TX processing.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos