Hi,
We'd like to know torelant of below impedance value.
How much % varies impedance value?
IOMUXC_SW_PAD_CTL_PAD_EIM_OE_B field descriptions
Drive Strength Field
Select one of next values for pad: EIM_OE.
000 HIZ — HI-Z
001 260_OHM — 157 Ohm @ 3.3V, 260 Ohm @ 1.8V
010 130_OHM — 78 Ohm @ 3.3V, 130 Ohm @ 1.8V
011 88_OHM — 53 Ohm @ 3.3V, 88 Ohm @ 1.8V
100 65_OHM — 39 Ohm @ 3.3V, 65 Ohm @ 1.8V
101 52_OHM — 32 Ohm @ 3.3V, 52 Ohm @ 1.8V
110 43_OHM — 26 Ohm @ 3.3V, 43 Ohm @ 1.8V
111 37_OHM — 23 Ohm @ 3.3V, 37 Ohm @ 1.8V
Regards,
Sugiyama
The tolerance of these impedance values is +/- 10%.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi, Artur,
Thanks,
Sugiyama