Max frequency of IPUx_CSIx_PIX_CLK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Max frequency of IPUx_CSIx_PIX_CLK

Jump to solution
593 Views
ko-hey
Senior Contributor II

Hi all

I want to confirm max frequency of IPUx_CSIx_PIX_CLK.

According to the section 4.11.10.3 of following data sheet, the max sensor clock frequency is 180 MHz.

http://cache.nxp.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf

However, it described that the maximum speed of the interface is 240 MHz in the section 38.1.2.1.1 of following reference manual

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf

Which one is correct ?

Ko-hey

Labels (1)
Tags (2)
0 Kudos
1 Solution
495 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

correct value is given in data sheet for every product part number,

reference manual gives generic IPU module values.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
496 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

correct value is given in data sheet for every product part number,

reference manual gives generic IPU module values.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
495 Views
ko-hey
Senior Contributor II

Hi Igor

Thank you for your quick support.

Ko-hey

0 Kudos