Hi all,
I am trying to write program to M4 core on my i.MX6SX. However so far I was unable to load any program.
Does anybody know what is wrong on following?
Prepare U-boot variables:
setenv fdt_file imx6sx-sdb-m4.dtb
setenv m4image m4_qspi.bin
setenv mmcboot 'run m4boot; echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;'
setenv mmcargs 'setenv bootargs no_console_suspend clk_ignore_unused uart_from_osc console=${console},${baudrate} root=${mmcroot}'
setenv spin_m4 'mw.l 0x7f8000 0x20008000;mw.l 0x7f8004 0x9;mw.l 0x7f8008 0xe7fee7fe;mw.l 0x20d8000'
setenv update_m4_from_sd 'if sf probe 1:0; then if run loadm4image; then setexpr fw_sz ${filesize} + 0xffff; setexpr fw_sz ${fw_sz} / 0x10000; setexpr fw_sz ${fw_sz} * 0x10000; sf erase 0x0 ${fw_sz}; sf write ${loadaddr} 0x0 ${filesize}; fi; fi'
setenv loadm4image 'fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${m4image}'
setenv m4boot 'sf probe 1:0; bootaux 0x78000000'
This is what I get after running update_m4_from_sd:
=> run update_m4_from_sd
SF: Detected N25Q256 with page size 256 Bytes, erase size 4 KiB, total 32 MiB
reading m4_qspi.bin
54948 bytes read in 29 ms (1.8 MiB/s)
Unknown command 'setexpr' - try 'help'
Unknown command 'setexpr' - try 'help'
Unknown command 'setexpr' - try 'help'
sf - SPI flash sub-system
Usage:
sf probe [[bus:]cs] [hz] [mode] - init flash device on given SPI bus
and chip select
sf read addr offset len - read `len' bytes starting at
`offset' to memory at `addr'
sf write addr offset len - write `len' bytes from memory
at `addr' to flash at `offset'
sf erase offset [+]len - erase `len' bytes from `offset'
`+len' round up `len' to block size
sf update addr offset len - erase and write `len' bytes from memory
at `addr' to flash at `offset'
SF: 54948 bytes @ 0x0 Written: OK
=>
I am confused at this point, because last line of output says "written, OK", but still there is error.
Why my U-Boot does not know setexpr?
Next issue is with booting M4.
setenv m4boot 'sf probe 1:0; bootaux 0x78000000'
setenv mmcboot 'run m4boot; echo Booting from mmc ...; run mmcargs;.........
=> boot
switch to partitions #0, OK
mmc2 is current device
switch to partitions #0, OK
mmc2 is current device
reading boot.scr
** Unable to read file boot.scr **
reading zImage
5979016 bytes read in 346 ms (16.5 MiB/s)
SF: Detected N25Q256 with page size 256 Bytes, erase size 4 KiB, total 32 MiB
Unknown command 'bootaux' - try 'help'<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<
Booting from mmc ...
reading imx6sx-sdb-m4.dtb
47253 bytes read in 20 ms (2.3 MiB/s)
Kernel image @ 0x80800000 [ 0x000000 - 0x5b3b88 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Using Device Tree in place at 88000000, end 8800e894
Starting kernel ...
Booting Linux on physical CPU 0x0
Why my U-Boot again does not know this command even if I get it from working manual?
Thank you in advance
Jan
Solved! Go to Solution.
It seems that you are using the community BSP. Please use the FSL/NXP BSP instead.
/Alejandro
Hi which bsp verion are you using?
Please check with the help command tha thte setexpre command exists as well as the bootaux command.
Best Regards,
Alejandro
Hi Alejandro,
I'm using 1.8 Fido.
U-Boot 2015.04+fslc+g5d9ffd2 (Nov 10 2015 - 00:45:50)
CPU: Freescale i.MX6SX rev1.2 996 MHz (running at 792 MHz)
CPU: Extended Commercial temperature grade (-20C to 105C) at 29C
Reset cause: POR
Board: MX6SX SABRE SDB
I2C: ready
DRAM: 1 GiB
PMIC: PFUZE100 ID=0x11
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment
In: serial
Out: serial
Err: serial
Net: FEC [PRIME]
Hit any key to stop autoboot: 0
=> setexpr
Unknown command 'setexpr' - try 'help'
=>
Unknown command 'setexpr' - try 'help'
=> bootaux
Unknown command 'bootaux' - try 'help'
=>
Unknown command 'bootaux' - try 'help'
=>
Unknown command 'bootaux' - try 'help'
=> help
? - alias for 'help'
base - print or set address offset
bdinfo - print Board Info structure
boot - boot default, i.e., run 'bootcmd'
bootd - boot default, i.e., run 'bootcmd'
bootm - boot application image from memory
bootp - boot image via network using BOOTP/TFTP protocol
bootz - boot Linux zImage image from memory
clocks - display clocks
cmp - memory compare
coninfo - print console devices and information
cp - memory copy
cpu - Multiprocessor CPU boot manipulation and release
crc32 - checksum calculation
dcache - enable or disable data cache
dhcp - boot image via network using DHCP/TFTP protocol
dm - Driver model low level access
echo - echo args to console
editenv - edit environment variable
env - environment handling commands
erase - erase FLASH memory
exit - exit script
ext2load- load binary file from a Ext2 filesystem
ext2ls - list files in a directory (default /)
false - do nothing, unsuccessfully
fatinfo - print information about filesystem
fatload - load binary file from a dos filesystem
fatls - list files in a directory (default /)
fatsize - determine a file's size
fdt - flattened device tree utility commands
flinfo - print FLASH memory information
fuse - Fuse sub-system
go - start application at address 'addr'
help - print command description/usage
i2c - I2C sub-system
icache - enable or disable instruction cache
iminfo - print header information for application image
imxtract- extract a part of a multi-image
itest - return true/false on integer compare
loadb - load binary file over serial line (kermit mode)
loads - load S-Record file over serial line
loadx - load binary file over serial line (xmodem mode)
loady - load binary file over serial line (ymodem mode)
loop - infinite loop on address range
md - memory display
mdio - MDIO utility commands
mii - MII utility commands
mm - memory modify (auto-incrementing address)
mmc - MMC sub system
mmcinfo - display MMC info
mw - memory write (fill)
nfs - boot image via network using NFS protocol
nm - memory modify (constant address)
pci - list and access PCI Configuration Space
ping - send ICMP ECHO_REQUEST to network host
pmic - PMIC
printenv- print environment variables
protect - enable or disable FLASH write protection
reset - Perform RESET of the CPU
run - run commands in an environment variable
saveenv - save environment variables to persistent storage
setenv - set environment variables
sf - SPI flash sub-system
showvar - print local hushshell variables
sleep - delay execution for some time
source - run script from memory
test - minimal test like /bin/sh
tftpboot- boot image via network using TFTP protocol
time - run commands and summarize execution time
true - do nothing, successfully
usb - USB sub-system
usbboot - boot from USB device
version - print monitor, compiler and linker version
=>
I don't see them in help.
BR
Jan
It seems that you are using the community BSP. Please use the FSL/NXP BSP instead.
/Alejandro
alejandrolozano what is the difference between the u-boot cloned from $ git clone git://git.denx.de/u-boot.git mentioned in u-boot on the i.MX6 sabre sd platform in a few commands and the one cloned from Freescale git repo cloned with $ git clone git://git.freescale.com/imx/uboot-imx.git
I ask because if I try to use the first one then bootaux is not found but it is found in the second one. It's confusing because I think there should be just one u-boot for Freescale boards.
Thanks!!