[K60ND512Z] Problems with the revision of silicon 1.8 8N30D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[K60ND512Z] Problems with the revision of silicon 1.8 8N30D

591 Views
josei
Contributor II

I have an application developed with MQX4.1 that works well in a micro K60ND512S 4N220.

I'm using the below setup:

  • psp_twrk60d100m (MQX4.1).
  • bsp_twrk60d100m (MQX4.1).
  • myApp for twrk60d100m.

When I want to run it on a microcontroller Rev. 8N30D not working.

What BSP and PSP files that I use?

Regards

0 Kudos
2 Replies

416 Views
josei
Contributor II

Gracias Soledad, puede resolver el problema.

Saludos

0 Kudos

416 Views
soledad
NXP Employee
NXP Employee

Hello José,

For devices with "Z" character (i.e. MK60DN512ZVMD10) it is necessary to clone the twrk60n512.

For devices without "Z" character (i.e. MK60DN512VMC10) it is necessary to clone the twrk60d100m

I hope this helps,
Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos