AnsweredAssumed Answered

imx28 with linux-3.0.35

Question asked by ???myir on Dec 9, 2015
Latest reply on Dec 10, 2015 by ???myir

Dear All,

 

The linux-2.6.35 is older version, so I would like to turn to linux-3.0.35, but it is not smooth.

 

Chosen Linux 3.0.35-imx from the menu of "./ltib -m config", then type ./ltib for building. I got the error message:

 

Processing: kernel-3.0.35
===========================
Build path taken because: build key set, no prebuilt rpm, 
Testing network connectivity
OK GPP: 

Try linux-3.0.35.tar.bz2.md5 from the GPP
http://bitshrine.org/gpp/linux-3.0.35.tar.bz2.md5:
15:37:40 ERROR 404: Not Found.
Try linux-3.0.35.tar.bz2 from the GPP
http://bitshrine.org/gpp/linux-3.0.35.tar.bz2:
15:37:40 ERROR 404: Not Found.
Can't get: linux-3.0.35.tar.bz2 at ./ltib line 802.


f_buildrpms() returned an error, exiting
traceback:
 main:572


Started: Wed Dec  9 15:37:33 2015
Ended:   Wed Dec  9 15:37:40 2015
Elapsed: 7 seconds

These packages failed to build:
kernel-3.0.35 

Build Failed

Exiting on error or interrupt

 

Ok, I thought the linux-3.0.35.tar.bz2 could not be downloaded. so I downloaded from:

linux-3.0.35.tar.bz2 [73.29 MiB] - MD5: 70bda6ecf3c498b23d2ced776479a8c3 - Fileinformation

and placed to /opt/freescale/pkgs directory, create the linux-3.0.35.tar.bz2.md5 manually, then run ./ltib again, got another error:

Processing: kernel-3.0.35
===========================
Build path taken because: build key set, no prebuilt rpm, 
Testing network connectivity
OK GPP: 

Try linux-3.0.35-imx_10.12.01.bz2.md5 from the GPP
http://bitshrine.org/gpp/linux-3.0.35-imx_10.12.01.bz2.md5:
17:00:32 ERROR 404: Not Found.
Try linux-3.0.35-imx_10.12.01.bz2 from the GPP
http://bitshrine.org/gpp/linux-3.0.35-imx_10.12.01.bz2:
17:00:33 ERROR 404: Not Found.
Can't get: linux-3.0.35-imx_10.12.01.bz2 at ./ltib line 802.


f_buildrpms() returned an error, exiting
traceback:
 main:572


Started: Wed Dec  9 17:00:29 2015
Ended:   Wed Dec  9 17:00:33 2015
Elapsed: 4 seconds

These packages failed to build:
kernel-3.0.35 

Build Failed

Exiting on error or interrupt

 

Hmmm...... now, the linux-3.0.35-imx_10.12.01.bz2 could not be download, and I could not find this file by google.

 

Could anyone provide some helps? Thanks in advance!

 

Best Regards,

Kinly,

Outcomes