AnsweredAssumed Answered

Can't play video using gstreamer 1.0

Question asked by ralph__ on Dec 9, 2015
Latest reply on Dec 10, 2015 by igorpadykov

I'm trying to play an MPEG4 video back using gstreamer-1.0 (having moved on from 0.10) but am having trouble with the command line:

 

# gst-launch-1.0 filesrc location=/usr/sample1080p30_40Mbps.mp4 typefind=true ! qtdemux ! imxvpudec ! queue max-size-buffers=3 ! imxipuvideosink

Setting pipeline to PAUSED ...

[INFO]  Product Info: i.MX6Q/D/S

Pipeline is PREROLLING ...

ERROR: from element /GstPipeline:pipeline0/GstQTDemux:qtdemux0: GStreamer encountered a general stream error.

Additional debug info:

qtdemux.c(4434): gst_qtdemux_loop (): /GstPipeline:pipeline0/GstQTDemux:qtdemux0:

streaming stopped, reason not-linked

ERROR: pipeline doesn't want to preroll.

Setting pipeline to NULL ...

Freeing pipeline ...

 

Any ideas what this error is about?  The equivalent command line worked fine on gstreamer-0.10.

 

Thanks, Ralph.

Outcomes