Linux 4.3 - Waiting for root device /dev/mmcblk0p1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux 4.3 - Waiting for root device /dev/mmcblk0p1

491 Views
angelobalke
Contributor II

I want to update my custom i.MX6 Board to Linux 4.3, but with the new Kernel the boot process stops at boot and can't load the rootfs from sd-card.

With the old Kernel 4.1.x it works fine with the same environment, only change is the newer Kernel.

U-Boot loads the Kernel from the sd-card, but the Kernel can't load the rootfs.

The mmc-support is enabled.

The sd-card is ext2 and ext2 support is enabled.

Boot message: http://pastebin.com/FdQ1KDaW

U-boot variables: http://pastebin.com/7Y8Gacdf

After I enabled the mmc debugging i get many messages, with whom I don't know what it means mmc debugging - Pastebin.com

Have I add some feature in the Kernel to get access to the sd-card or something other?

I activated all supports described in i.MX_6_Linux_Reference_Manual.pdf - 34.2.2 34.2.2 Menu Configuration Options - Pastebin.com

Best regards Angelo

Labels (3)
0 Kudos
0 Replies