Hi! I was planning to use in one of my projects Coldfire V4 MCF54415 processor. I had a few questions:
1) Where can I find USB Host Stack for this processor?
2) If he does not exist, how can I write own USB Stack?
Solved! Go to Solution.
If you are using an RTOS then you could ask your vendor. If not, then Freescale provide an RTOS with an integrated USB Host Stack for free: MQX USB Host/Device Stack|NXP . The MCF54415 is supported on the current release which is V4.2.
Good luck with your project.
Regards, Shaun
If you are using an RTOS then you could ask your vendor. If not, then Freescale provide an RTOS with an integrated USB Host Stack for free: MQX USB Host/Device Stack|NXP . The MCF54415 is supported on the current release which is V4.2.
Good luck with your project.
Regards, Shaun