AnsweredAssumed Answered

How do I set up an event handler for FTM / PWM fault interrupts with SDK 1.3?

Question asked by Lance Fisher on Dec 8, 2015
Latest reply on Dec 9, 2015 by xiangjun.rong

I'm trying to migrate a project from a DSP  and CW / PE to a Kinetis KV series part using KDS and SDK.  In the original code I had an event handler for faults on the PWM / timer peripheral and I can't find anything in the SDK API (Driver or HAL) that supports this for the FTM peripheral.   The only way I can see to implement this is a bunch of direct accesses to the FTM hardware registers which would defeat the whole purpose of the SDK.  Anyone have a better idea?

 

BTW, I'm also finding that the documentation for the SDK API is extremely inadequate (KSDK13APIRM) and the help function in KDS is even worse.  Is there any better documentation for the SDK API?

Outcomes