AnsweredAssumed Answered

Are the i.MX6 GPIOs fail safe?

Question asked by m.c on Dec 7, 2015
Latest reply on Dec 7, 2015 by m.c

For example, are they hi-Z when i.MX6 is powered off?  If I had a 10KΩ pull-up to 3.3V on one of the i.MX6 GPIO pins, would I expect the pin to stay high when the i.MX6 is powered off?  It’ll depend on the I_OFF leakage on the pin or the ESD structure.

Outcomes