mx287: use mfgtool to update firmware fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mx287: use mfgtool to update firmware fail

900 Views
hwo
Contributor III

Hi all,

when burn the board through otg port, the process fail.

partial console trace is :

dcp dcp.0: DCP crypto enabled.!

usbcore: registered new interface driver hiddev

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

ALSA device list:

  No soundcards found.

TCP cubic registered

NET: Registered protocol family 17

can: controller area network core (rev 20090105 abi 8)

NET: Registered protocol family 29

can: raw protocol (rev 20090105)

regulator_init_complete: incomplete constraints, leaving vbus5v on

mxs-rtc mxs-rtc.0: setting system clock to 1970-01-01 00:00:27 UTC (27)

Freeing init memory: 176K

init started: BusyBox v1.15.0 ()

starting pid 1082, tty '': '/etc/rc.d/rcS'

Mounting /proc and /sys

Setting the hostname to freescale

Mounting filesystems

mount: mounting shm on /dev/shm failed: No such file or directory

mount: mounting usbfs on /proc/bus/usb failed: No such file or directory

Starting inetd:

starting pid 1109, tty '': '/sbin/getty -L ttyAM0 115200 vt100'

process '/sbin/getty -L ttyAM0 115200 vt100' (pid 1109) exited. Scheduling for restart.

starting pid 1110, tty '': '/sbin/getty -L ttyAM0 115200 vt100'

process '/sbin/getty -L ttyAM0 115200 vt100' (pid 1110) exited. Scheduling for restart.

MFGTOOL log and the ucl.xml contents are:

Friday, December 04, 2015 17:34:05

1 - Panel A Start processing SPI-NOR (kernel only) <LIST/>.

Panel A Start <CMD/> type="boot" body="Recovery" file="updater.sb" timeout="10" onError="" text="Booting update firmware.".

1 - Panel A Finished <CMD/> type="boot" body="Recovery" file="updater.sb" timeout="10" onError="" text="Booting update firmware." SUCCESS code=0x0.

Panel A Start <CMD/> type="boot" body="Recovery" file="updater_ivt.sb" timeout="10" onError="" text="Booting update firmware.".

1 - Panel A Finished <CMD/> type="boot" body="Recovery" file="updater_ivt.sb" timeout="10" onError="" text="Booting update firmware." SUCCESS code=0x0.

Panel A Start <CMD/> type="find" body="Updater" file="" timeout="180" onError="" text="".

Panel A UtpUpdate Event: DeviceRemoval Msg: (null) DevState: Disconnected OpState: WAITING_FOR_DEVICE

Panel A Current state: 10

1 - Panel A Finished <CMD/> type="find" body="Updater" file="" timeout="180" onError="" text="" FAIL code=0xffff0006.

Panel A: Operation is timeout.,failed to run command: type="find" body="Updater" file="" timeout="180" onError="" text="" 

2 - Panel A Finished processing SPI-NOR (kernel only) <LIST/> : FAIL code=-65530.

Panel A: Reason is unknown,

<LIST name="SPI-NOR (kernel only)" desc="test">

<CMD type="boot" body="Recovery" file="updater.sb" if="HabDisable">Booting update firmware.</CMD>

<CMD type="boot" body="Recovery" file="updater_ivt.sb" if="HabEnable">Booting update firmware.</CMD>

<CMD type="find" body="Updater" timeout="180">

<CMD type="push" body="mknod class/mtd,mtd1,/dev/mtd1"/>

<CMD type="push" body="$ flash_eraseall /dev/mtd1">Erasing kernel partition</CMD>

<CMD type="push" body="send" file="files/imx28_ivt_linux.sb">Sending kernel</CMD>

<CMD type="push" body="$ dd if=$FILE of=/dev/mtd1">Programming kernel</CMD>

<CMD type="push" body="$ echo Update Complete!">Done</CMD>

</LIST>

Could be the usb driver's problem or something else? What does the find command exactly do during the 180 seconds waiting?

Many thanks

Labels (2)
0 Kudos
1 Reply

436 Views
igorpadykov
NXP Employee
NXP Employee

Hi h

please look at ucl.xml and other linux patches describing spi-nor usage with i.MX28

How to enable SPI NOR boot for i.MX28 (Spansion s25fl256s)

you may be interested to look at mxsldr tool:

http://git.denx.de/?p=mxsldr.git;a=summary

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos