i.mx6UL in automotive temperature range?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6UL in automotive temperature range?

523 Views
farangutan
Contributor I

Does Freescale plan to offer a i.mx6UL processor in an automotive temperature (-40C to +85 C)  range?

if so, when?  If not, are other there processor in the i.MX6 family (SL?) that might be offered in extended

temperature range?

Thanks,
Wayne

Labels (1)
0 Kudos
1 Reply

386 Views
igorpadykov
NXP Employee
NXP Employee

Hi Wayne

UL automotive version is planned on 1Q2016

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos