Hi,
We are using KDS to create libraries which we use on both M4 and M0+, and they all exist in Debug and Release versions.
Today I found that my M4-Debug version (M4-Debug\mmSrc\MMComm\subdir.mk) has more files than the M0-version!!!
It seems that the subdir.mk is only updated on the actual build target?
Is this right or am I missing something?
Hi,
subdir.mk is Automatically-generated file after build.
can you please:
1. manually remove it from your project folder.
2, do "project", "clean..." then rebuild your project. this can generate a new subdir.mk file.
can it work for you?
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------