AnsweredAssumed Answered

KL25Z Traffic Light Program - Code and Breadboard Issues

Question asked by Dan Cymbala on Dec 4, 2015
Latest reply on Dec 10, 2019 by JODAN LEONG

Essentially, what I'm trying to do is have lights cycle through 3 corresponding LEDs on the breadboard via some ARM assembly code on the KL25Z using Keil uVision 5 as my IDE. I've chosen PIN PTA2 to be my green LED, PTA4 to be my yellow, PTA5 to be my red, PCR7 to be emergency reset button which restarts the cycle at green (I haven't implemented this in code yet since I haven't even gotten the cycle to work) -- details are commented in the code. No LEDs are being lit up and I'm curious as to why. Here is my code:

 

 

SIM_SCGC5   EQU  0x40048038 ;SIM_SCGC5 address  
SIM_COPC     EQU  0x40048100 ;SIM_COPC (watchdog) address
    
PORTA_PCR2  EQU  0x40049008 ;PORTA_PCR2 (PTA2) address
PORTA_PCR4  EQU  0x40049010 ;PORTA_PCR4 (PTA4) address
PORTA_PCR5  EQU  0x40049014 ;PORTA_PCR5 (PTA5) address
PORTC_PCR7  EQU  0x4004B01C ;PORTA_PCR7 (PTC7) address

PORTA_PDDR  EQU 0x400FF014
PORTA_PDOR  EQU 0x400FF000
PORTC_PDDR  EQU 0x400FF094
PORTC_PDIR  EQU 0x400FF090
    
GREEN_MASK   EQU 0x00000004 ; PORTA_PIN 2
YELLOW_MASK  EQU 0x00000010 ; PORTA_PIN 4
RED_MASK     EQU 0x00000020 ; PORTA_PIN 5
INIT_MASKS   EQU 0x00000034 ; PORTA_PIN 2, 4 and 5
BUTTON_MASK  EQU 0X00000080 ; PORTC_PIN 7
DELAY_CNT    EQU 0X00800000

    AREA asm_area, CODE, READONLY 
    EXPORT  asm_main 
asm_main  ;assembly entry point for C function, do not delete 
; Add program code here 
    BL init_gpio  
loop 
    BL greenon
    LDR R0, =DELAY_CNT
    BL  delay
    BL  redon
    LDR R0, =DELAY_CNT
    BL  delay
    BL  yellowon
    LDR R0, =DELAY_CNT
    BL  delay
    B   loop
greenon
    LDR R0,=PORTA_PDOR  ;Load address of PORTA_PDOR to R0 
    LDR R1,=GREEN_MASK    ;Load value to R1 
    STR R1,[R0]     ;Put value into PORTA_PDOR
    BX LR

redon
    LDR R0,=PORTA_PDOR  ;Load address of PORTA_PDOR to R0 
    LDR R1,=RED_MASK    ;Load value to R1 
    STR R1,[R0]     ;Put value into PORTA_PDOR
    BX LR

yellowon
    LDR R0,=PORTA_PDOR  ;Load address of PORTA_PDOR to R0 
    LDR R1,=YELLOW_MASK    ;Load value to R1 
    STR R1,[R0] ;Put value into PORTA_PDOR
    BX LR

delay
    SUBS R0, #10
    BNE  delay
    BX LR

init_gpio 
    ;Disable watchdog timer (COP) 
    LDR R0,=SIM_COPC
    LDR R1,=0x0
    STR R1,[R0]
    
    ;Turns on clocks for all ports 
    LDR R0,=SIM_SCGC5    ;Load address of SIM_SCGC5 to R0 
    LDR R1,[R0]          ;Get original value of SIM_SCGC5 
    LDR R2,=0x00003E00   ;Load mask for bits to set to R2 
    ORRS R1,R2           ;Set bits with OR of orig val and mask 
    STR R1,[R0]          ;Put new value back into SIM_SCGC5

    ; Setup PORTA Pins 2,4 and 5 to be outputs
    LDR R0,=PORTA_PDDR   ;Load address of PORTA_PDDR to R0 
    LDR R1,=INIT_MASKS    ;Load new value to R1 
    STR R1,[R0]           ;Put value into PORTA_PDDR 

    ; Setup PORTC Pin 7 to be an input
    LDR R0,=PORTC_PDDR ; Load address of PORTC_PDDR to R0 
    LDR R1,=BUTTON_MASK     ;Load new value to R1 
    STR R1,[R0]            ;Put value into PORTC_PDDR


    BX LR

    END


Any help/suggestions would be immensely appreciated! Thanks in advance.

Attachments

Outcomes