mx6ul platform sii902x hdmi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mx6ul platform sii902x hdmi

2,250 Views
bingking88
Contributor I

Hi fsl

in imx6ul-14x14-ddr3-arm2.dts

sii902x config:

   sii902x_reset: sii902x-reset {

                compatible = "gpio-reset";

                reset-gpios = <&gpio1 23 0>;

                reset-delay-us = <2000000>;

                #reset-cells = <0>;

        };

&i2c2 {

        clock_frequency = <100000>;

        pinctrl-names = "default";

        pinctrl-0 = <&pinctrl_i2c2>;

        status = "okay";

        sii902x@39 {

                compatible = "SiI,sii902x";

                reg = <0x39>;

                interrupt-parent = <&gpio1>;

                interrupts = <18 2>;

                mode_str ="1024x768M@60";

                bits-per-pixel = <16>;

                resets = <&sii902x_reset>;

        };

};

i2c pin config:

pinctrl_i2c1: i2c1grp {

                        fsl,pins = <

                                MX6UL_PAD_GPIO1_IO03__I2C1_SDA  0x4001b8b1

                                MX6UL_PAD_GPIO1_IO02__I2C1_SCL  0x4001b8b1

                        >;

                };

                pinctrl_i2c2: i2c2grp {

                        fsl,pins = <

                                MX6UL_PAD_CSI_HSYNC__I2C2_SCL  0x4001b8b0

                                MX6UL_PAD_CSI_VSYNC__I2C2_SDA  0x4001b8b0

                        >;

                };

system log print:

sii902x 1-0039:  Sii902x: cound not find device

the drivers/video/mxc/mxsfb_sii902x.c

/* Set 902x in hardware TPI mode on and jump out of D3 state */

        if (i2c_smbus_write_byte_data(sii902x.client, 0xc7, 0x00) < 0) {

               dev_err(&sii902x.client->dev,

                        " Sii902x: cound not find device\n");

            return -ENODEV;

       }

hardware test power supply reset were normal

can you give some advice

tks!

Labels (4)
Tags (1)
0 Kudos
4 Replies

1,153 Views
igorpadykov
NXP Employee
NXP Employee

Hi bingking

please refer to attached i.MX 6UltraLite EVK Board Hardware

User’s Guide sect.2.21 HDMI display connector (J1001) how to

use hdmi.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,153 Views
bingking88
Contributor I

hello igorpadykov

     the board is our custom made ,chip has welding, signals test are normal !

     i2c test is ok

     but if (i2c_smbus_write_byte_data(sii902x.client, 0xc7, 0x00) < 0)  error!

whether in the public version of the transplanted over sii902x code?

thank you very much!

0 Kudos

1,153 Views
igorpadykov
NXP Employee
NXP Employee

based on error: Sii902x: cound not find device\n"

seems device is not found, you can check i2c signals with oscilloscope

~igor

0 Kudos

1,153 Views
bingking88
Contributor I

hardware signals no problem,Can not determine whether the software config OK

the above  dts config

tks!

0 Kudos