I am new to this types of file.
How to start with writing to the files..
Hello
what chip and CW version do you work with?
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I am working with MC56F82748 DSC Controller..
Right now I am working with Bootloader for this controller.
I am having two files..
1. Bootloader file
2. My application file
To run the apllication using bootloader, i need to change .cmd file of the My application file..
Kindly help me..
Hello Ramakrishna
The new created barebord project in CodeWarrior already includes a link command file, if user needs to modify it, please refer to <Chapter 7 ELF Linker> in the document below for its syntax.
C:\Freescale\CW MCU v10.6.4\MCU\Help\PDF\MCU_DSC_Compiler.pdf
The application which is loaded by bootloader should meet some requirements. It should use different flash pages with bootloader. And user may write its entry point and bootloader start delay time in link command file.
This document should be helpful to you:
http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4759.pdf
Best Regards
Fiona Kuang
Technical Information & Commercial Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------